80Mpa以上の荷重がかかるアプリケーションでは、熱可塑性材料製のすべり軸受が限界に達することがあります。イグスは、新しいigutex繊維巻き軸受シリーズで既存の標準すべり軸受の製品ラインアップを拡大しました。このシリーズは、建設機械やホイストなどの重責務エリアでその強さを発揮します。製品ファミリーの最新開発は、igutex TX3という素材です。従来のigutexベアリングよりも高い荷重に対して、より高い性能を提供します。
食品加工業界の機械では、薬品による清掃が日常的に行われています。わずかな隙間に水分が溜まってしまい、機械内の汚染につながることもあります。そのため、衛生設計を重視した部品設計を行う事業者が増えてきています。イグスはEHEDGのメンバーであり、衛生設計ガイドラインに基づいた最初のリニアガイドシステムを開発しました。高機能ポリマー「イグリデュールA160」、ステンレス鋼、洗浄可能なキャリッジの内部など、FDAに準拠した素材を使用し、衛生的な設計を徹底しています。